Other Parts Discussed in Thread: TUSB8040A1
Hello,
I'm using the TUSB8040A1 as part of a design that requires 14 downstream USB 3.0 ports. I have an issue, all the downstream ports work but only in USB2.0 mode. The cables on the two uptsream ports are connected on the SuperSpeed ports of my computer. The A11 output (HS) is enable and not the A12 output (SS) on each TUSB8040A1.
The design is based on the EVM.
I can provide my schematic to debug my issue.
Thanks
Pierre-Yves