Other Parts Discussed in Thread: TLK10232
Hi Sir:
Environment setting as follows.
The external OSC is 156.25MHz for 10G-KR.
The SFP+ Copper connect to 10G switch.
The other switch doesn't display link up function.
Could you provide solution or PHY initial code to me how to debug?
1E.000F
[3] RX_LS_OK
[2] TX_LS_OK
[1] LS_PLL_LOCK
[0] HS_PLL_LOCK
MDIO#1 PHY=0, DEV=0x1e(30), REG=0x000f(15): 0x191b
MDIO#1 PHY=0, DEV=0x1e(30), REG=0x000f(15): 0x191b
We try to enable PCS loopback (03.0014), and disable AN (07.0000) and LT (01.0096).
The channel status 1E.000F[3:0] is still 0x3. i.e. still not link up.
Thank you for your support.