Other Parts Discussed in Thread: MAX202
Hi,
Can anyone help to resolve below issue.
We have seen the following issue in HPAC04 RS232 circuit using MAX202.
The RX & TX from microcontroller(MC9S08PA60) to the MAX202 has overshoots at the transitions of these digital signals. Also there are spikes on RX line when TX is being transmitted and vice versa. These overshoots are exceeding the limits of the ICs(5.5V). The circuit is designed as recommended in the datasheets.
Attached schematics and waveforms for your reference.
Rgds,