Other Parts Discussed in Thread: SN65LVPE512, TUSB551, TUSB501
Dear Specialists
My customer is evaluating SN65LVPE512 for device side.
He has already confirmed URL.
http://e2e.ti.com/support/interface/usb/f/1008/t/450944
In the condition, he encountered some problems.
Could you please advise.
1. It was not recognized between host(PC) and device(SN65LVPE512) by USB2.0 cable.
USB controller of device side is EZ-USB FX3(cypress).
SN65LVPE512 is in front of the EZ-USB FX3.
It is recognized if the connection is cut USB3.0 physically.
He thinks the device should be normally passed both USB2.0 and USB3.0.
2. The device could not be in the Rx compliance test, therefore he couldn't test.
If SN65LVPE512 is removed, it can be in the compliance mode.
He is thinking that SN65LVPE512 is originally for host.
If it is used for device, it is needed not only changing connection, but also another points for instance power sequence or etc.
Could you please see an attached file.
Best regards,
Shinichi