Other Parts Discussed in Thread: SN65LVPE502A, SN65LVPE512
Dear Specialists,
MY customer is evaluating with SN65LVPE502B, EZ-USB FX3(cypress) and PC.
Depend on the connect sequence of 3 devices, USB2.0 connection is not recognized.
The phenomenon is occurred not only SN65LVPE502B, but also SN65LVPE502A and SN65LVPE512.
Could you please advise the reason and the solution?
TEST Condition
EZ USB -> USB3.0 Cable -> SN65LVPE502BEVM -> USB2.0 Cable -> PC
Power supply of 502B is self powered 3.3V. (Vbus is not using)
EN is ON at the same time.
(1)Connection Sequence 1 USB2.0 recognition is NG
1. connect EZ USB and SN65LVPE502BEVM
2. connect SN65LVPE502BEVM and PC
This is similar to Device side connection.
(2)Connection Sequence2 USB2.0 recognition is OK
1. connect SN65LVPE502BEVM and PC
2. connect EZ USB and SN65LVPE502BEVM
This is similar to Host connection.
When these devices use device side, it may require a little ingeuity
I appreciate your great help.
Best regards,
Shinichi