Other Parts Discussed in Thread: TUSB2077A
Hi,
We have been designing a 7-port USB Hub to support high current requirements at down stream. But i could see from TUSB2077A EVM user guide section 4.1 that in Bus Power mode it can only support up to 4 downstream ports & if we want to use more down stream ports then we should also use Wall Wart ( DC Jack). Is that true? I am attaching our schematic for this purpose. Can you please give me some suggestions on this. In between we are designing to support 2A for 4 of the down stream ports and other ports are with lower current support.
Thanks
SreeTUSB 2077A.PDF