Other Parts Discussed in Thread: DP159RGZEVM
How to configure the DP159RGZEVM board output HDMI if only AUX_P/N(there is no DDC clock and data from GPU ) output support in GPU?
Does the I2C over AUX feature of DP159 need enable for this support?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DP159RGZEVM
How to configure the DP159RGZEVM board output HDMI if only AUX_P/N(there is no DDC clock and data from GPU ) output support in GPU?
Does the I2C over AUX feature of DP159 need enable for this support?
Hi Moises:
Let me explain our configuration and our request.
In our module, the limitation of DDI0 channel is we didn’t connect DDC_CLK/DATA to ROW connector. We just have DDI0_AUXP/N to Row connector.
So we want to use DP159 DP to HDMI ouput without DDC_CLK/DATA signal.
We have DP159RGZEVM board with our module to test it.
Unfortunately, we can't output HDMI screen until now.
Below is our experiment configuration:
Un-Pop:
R127, R31, R32, R132, R133,
POP:
C2, C3
I2C_EN: Low or NC
HDMI_SEL: Low or NC
Power: from power supply 5V
SW2: 1-2
Based on upon setting, the HDMI screen still can’t output.
Please help us to clarify this issue.
Please give us a right configuration in DP159RGZEVM board.
Thx~
Hi Hsieh,
AUX bridge is enabled by default, have you tested EVM with a different device like a computer to make sure the EVM is working?
Regards
Hello Moises,
Quick question:
The Neo wourl like to know that does DP159 support HDMI output without DDC(SDA_SRC/SCL_SRC).
there is only AUX channel(No DDC) support in GPU.
There is no display problem if connect DDC and AUX with DP159EVM. The problem only happen if only connect with AUX channel only.
Hi Peter,
I got it, the GPU is unable to send I²C over AUX.
Then the problem is not in DP159, you may use DP159 without DDC, just some controller will have to take care of TMDS_CLOCK_RATIO.
The problem is: DP++ doesn't send video by default when DDC is not present, HDMI send video by default when DDC is not present.
So, if there is no DDC Source will not send video to sink.
Regards
Hi Moises:
Thank your help.
I have three questions need your confirmation.
1. So if there is no DDC Source support in the DP++ source end, the DP159 will not send video to sink.
=> It means the DP159 need DP dual mode, right?
=> DP159 can’t support only pure DP channel, right?
2. DP++ doesn't send video by default when DDC is not present, HDMI send video by default when DDC is not present
=> It means if source is HDMI signal, it can output screen when DDC is not present, right?
=> DDC_CLK/DAT is not present, how can screen display correct pixel resolution?
3. Based on our configuration, our DDI0 channel is pure DP, not DP dual mode(because no DDC_CLK/DATA), but we need to screen output HDMI device.
Which chipset can recommend from TI?
Thx~~
The DP159 support DP++ dual mode to HDMI only. It does not support pure DP input.
Hi Hsie, Peter,
First for Hsieh questions, let's clarify this DP/DP++ difference.
DP is just the standard DisplayPort interface using 4 differential pairs for video and AUX channel for configuration.
DP++ sends HDMI data using DP electrical signaling(AC coupled), that's why you need a level shifter from DP++ to HDMI.
Presence or absence of DDC is not what differentiates from DP to DP++.
Since you want HDMI output, you need DP++ with a level shifter. Another option could be a protocol converter from DP to HDMI(We don't have it)
I mentioned DP++ needs DDC channel because we are talking about this application, but DP needs it AUX channel too.
HDMI send video by default when DDC is not present, in this case source sends a default resolution it doesn't send the correct resolution.
Although DP159 is advertised as DP++ to HDMI level shifter, it can be used as DP to DP retimer.
If you are interested in this application, please refer to application note DP159 as DisplayPort retimer http://www.ti.com/lit/an/slla358/slla358.pdf
Regards