Other Parts Discussed in Thread: DS90C031QML-SP, STRIKE
The DSCC 5962-95833 spec lists, in the absolute maximum ratings section, the output voltage (Dout+, Dout-) as -0.3V to (Vcc+0.3). Does Vcc in (Vcc+0.3V) mean the applied Vcc -- i.e., the actual supply voltage of part in the circuit? For a 5962R9583301VFA device that is off (not powered, Vcc = 0V), is the 5962R9583301VFA part stressed if one of the +/- outputs inadvertently sees 3.3V?