Other Parts Discussed in Thread: TPS2511, TPS2513, TPS2514, TPS2546
Hi,
I have been using the TPS2511 for a USB charger for several years now. I recently embarked on a program to increase the charge current from about .5A to 1A+. I am finding that the DP/DM shorted mode + 1.2V does not seem to be detected properly by a Google Nexus 7 tablet.
The USB charger is part of a solar system that provides USB charging among other things. One goal is to provide the best charging experience for as many devices as possible. This Nexus 7 tablet is actually the only device I have tested against that I have verified requires shorted + 1.2V.
I do have the DM/DP lines swapped to impliment a 5W divider configuration. It appears to have something to do with the timing and or possibly seeing DM/DP shorted w/o the bias.
The TPS2511 seems to be the best solution for a dedicated charger ID but I am open to suggestions.
Any comments or thought would be much appreciated.
Regards
Larry