Other Parts Discussed in Thread: TCA9406
Hi,
My I2C connection schema is explained in detail in the attached pdf (2 page)
We have developed module 2 which works on 3.3V , the I2C on this device always operates in slave mode. We are interfacing this to other modules(modules 1 &3) which are working on 5V logic. Module 1 serves as I2C master.
Therefore we used TI TCA9406 for I2C voltage level conversion to interface the other modules to our module. I have pulled OE permanently and also connected the same pin to Micro GPIO on module 2
Refer to Page 1: The I2C connection schema is explained. In this configuration the I2C works perfectly OK. The problem is when we connect another device Module 3(refer page 2)
Refer to Page 2: I2C connection schema explained. In this mode the I2C doesn't communicate with the slave device on module 2. For isolating the problem, we have removed level translator on Module 2 and directly shorted the I2C bus of our module with the external I2C and it works perfectly fine. We have a doubt if the internal pull up resistors in this level translator device is creating problem?
Please review and suggest.
I2C Query.pdfRegards
Ravi