Other Parts Discussed in Thread: TUSB2046B
Hello to everyone,
i would like to use the TUSB2046BITexas_Instruments-TUSB2046BIVFR-datasheet.pdf in my design for controlling two modems (USB Signals) but unfortunately i have to use the same USB Bus. For this reason i decided to use the tub2046 bi (the onlyone that has industrial specifications even if i need only two USB ports instead of 4). However because of the big current values that the two modems need i do not need to use the PWR_ON and the OVRCUR signals at all.
Would it be a problem if i leave the PWRON not connected and the OVRCUR connected with Ground or would it make it difficult to use the ic that i chose?
attached you will find the datasheet of the IC.
Many thanks George.