This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: DS90UB914A/934 deserializer compatibility with DS90UB953 serializer

Part Number: DS90UB954-Q1


We are working on a project where a new camera board with a MIPI image sensor and a DS90UB953 serializer will be communicating with a DS90UB914A deserializer. I see that these parts should be able to communicate with each other. I found this forum thread asking about the compatibility of the DS90UB933 with the DS90UB954 and I would like some clarification: 

e2e.ti.com/.../545411

1) Is the DS90UB953 compatible with the DS90UB914A?

2) MIPI data input to the 953 fed across the FPDLink III connection will be converted to parallel data out of the DS90UB914A?  

3) What are the restrictions on the DS90UB953 when running in this mode? 

4) What are the restrictions on the DS90UB914A when running in this mode? 

The camera design is using all four MIPI data lanes and the camera is running 1280 X 1080 @ 30fps. 

Thank You,

 Ben Missele