Part Number: DP83848K
Other Parts Discussed in Thread: TEST2
We are using the DP83848K IC & recommended Connector : Pulse J0011D21B.
Our board is working with Ethernet speed of 10Mb/s but does not work with the 100Mb/s.
Testing Process:
1) On Board Boot up auto-negotiation is ON so default speed is set the 100Mb/s. but does not send any packet to remote server which was connected with the board over LAN.
2) We have set auto-negotiation is OFF and speed is 100Mb/s using the ethtool. but still does not send any packet to remote server which was connected with the board over LAN.
3) We have set auto-negotiation is OFF and speed is 10Mb/s using the ethtool. it will send and receive packets over LAN.
Please help us to solve or debug issue as soon as possible.
Thanks in advance.