Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: Board not Bring-Up with USB cable

Part Number: TUSB4020BI

Hi all,

I our design we are using USB hub, this hub interface working good (Device connected to battery ).

without battery the board is not bring up(USB cable connected to our PC).

Supply VDD=1.1V

Supply VDD33=3.3V

I am isolating in our design major power supplies except USB hub supply.

This USB hub Consumes current  at VDD=54mV,VDD33=50mV(both battery and USB cable connected to our device),

without USB hub board is bring up(isolating USB hub supply remain all power supplies connected ) (condition Battery not connected only USB cable is connected to my Device)

Thanks,

Siva.