Part Number: TPS2511
I designed a simple USB pass through device utilizing the TPS2511 that allows me to control the current draw of a connected device while it is charging. It works fine for Android devices, but when I try it with Apple device (iPhone/iPad) and set the current limit above 100 mA, I get the following warning:
"This accessory may not be supported"
The Apple device then limits the current draw to 100 mA no matter what value I set the ILIM_SET resistor to. I've attached a schematic of the design. Anyone have any ideas what is going on? Could it be related to the ESD protection devices?USB_Charger.pdf