Part Number: TPS65982
Hi all,
I would like to ask you if it's possible to select a more suitable PDO than the highest /Voltage|Current|Power one?
Let's consider this example:
I have a sink that can accept from 6 to 20V. My charger can provide 5, 9, 12, 20V.
My sink negotiation policy is the following one: choose the highest voltage.
But in my application i would prefer a 9V contract. Can I somehow force my sink to chose this contract instead of the highest voltage/current/power one?
Do I have to uncheck "Autonegotiate Sink" and sthg else? Which registers should i manipulate to change it?
Thanks in advance,
Daniel