Part Number: DP141RLJEVM
Other Parts Discussed in Thread: TUSB546-DCI
Dear SIr
Our test structure as below
DP source => 5m cable => DP141EVM => 5m cable => Agilent W2641B
Use EVM default setting but the result is fail ,test report as below
Please kindly help to confirm
1. We test DP141EVM ,but DP141 EVM default setting have many test fail ,test report as attached file
Do you have the test report for DP1.2b??
(test environment is 5m cable to DP141EVM to 5m cable ) and PS8460EVM pass all of test
2. We find DP141 EVM doesn’t have resistor on the EVM
Do you have recommend setting guide for different cable condition ? or application note for cable ?
3.What’s large input swing’s mean ?
Does it mean if use DP141 for large input swing ,DC GAIN need to set -6dB ?
4. Compatibility test result (red words means can't display output)