Hey,
I'm using TPS2051B in one of my circuits.
Currently I'm investigating on possible risks of damaging this IC due to some special conditions.
The problem:
There are some special conditions on my system, where supply voltage is powered off for this IC (IN-pin = 0V).
However, I'm not able to fully control the EN-pin. It is possible that this line has a logic high state (EN-pin = 3.3V), even when power is off (IN-pin = 0V).
I searched in the datasheet, but was not able to find any information about the maximum values of this pin, when power is off.
Does anyone know if there are possible risks to damage the IC or where I can find this information in the datasheet.
Thanks in advance!
Greetings, NM