This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO3130: Daisy-chain connection of PCIe Packet Switch

Guru 15520 points
Part Number: XIO3130


Hi,

I have a question about XIO3130 PCIe packet switch.

In our system, there are one Master board and eight independent sub board.
We are planning to connect the master board and each sub board via PCIe.
So, we are searching for packet switch which can fanout 8 outputs.

It seems XIO3130 is the only packet switch product in TI,
and XIO3130 only support 3 fanout.
Is it possible to realize 8 fanout by using a few XIO3130?
For example connecting a few XIO3130 by daisy-chain connection.

best regards,
g.f.