Part Number: TCA9544A
Other Parts Discussed in Thread: TMP464
Hi Sirs,
We have use TCA9544A +TMP464
1. Could you help double check schematic?
2. TCA9544A INT0-3 could use one PU resistor?
Thanks!!
Schematic:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Shu-Cheng,
Everything on our device looks good. The device address is correct at 0x70h.
1) Just to be sure you have pull up resistors tied to SDA/SCL_BL(1,2,3,4).
2) INT0,1,2,3 are okay to have one pull up resistor.
3) The 10uF caps are a bit of an overkill. You don't need that much. It should still work though.
Thanks,
-Bobby