Part Number: TUSB9261-Q1
Other Parts Discussed in Thread: TUSB9261,
Hello,
Would you please answer the following questions regarding TUSB9261 - Q1?
1.About the description of TUSB9261-Q1 data sheet (SLLSEE 2A) P.12 Power Up and Reset Sequence
(Q1) It is written at the beginning of this chapter that there is no specification for VDD, VDD33, VDDA33 power sequencing.
However, in the second half, it is written to raise VDD before VDD33 or at the same time.
which one is correct?
> The TUSB9261-Q1 does not have specific specific power sequencing requirements with respect to the core power
> (VDD), I / O power (VDD 33), or analog power (VDDA 33) for reliability reasons.
> If a passive reset circuit is used to provide GRSTz
> It is recommended that core power (VDD) be ramped prior to or at the same time as I / O power (VDD 33).
(Q2) There are two descriptions about the reset time of GRSTz,
Which is correct, "MIN 1ms" or "greater than 2 ms but less than 100 ms" ?
> A minimum reset duration of 1 ms is required.
> The recommended duration of the GRSTz input is greater than 2 ms but less than 100 ms.
(Q3)Are there any specifications to be complied with regarding the power "down" sequencing of each power supply?
2. About VSSOSC
(Q1) When using crystal, it is written in the data sheet that VSSOSC needs to be floated from GND.
How should I handle the inner layer of the lower substrate of the crystal?
Usually, I think there is a GND plane there.
(Q2)Woule you please tell me the concern when using crystal and connecting VSSOSC to GND?
3.SATA communication after BOOT
(Q1)I think that the IC negotiates on the SATA side after completing Boot and establishes communication.
Will it run automatically after startup?
4.TUSB9261-Q1 Internal register map
(Q1)Can I have an internal register map for this device?
Best Regards,Orobianco.