Part Number: DP83849I
Tool/software: Linux
Hello! When we use imx6ul to connect to dp83849i and transmit data with TFTP, we have errors such as error frame: 0x9ef21380 0x00000810. U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b942 May I ask what kind of problem is it?
If "Ping" is used basically, this error will not occur.
Circuit schematic and error records are found in the appendixDTU_MB_171208.pdf
TFTP from server 192.168.10.10 ; our IP address is 192.168.10.100 Filename 'u-boot.bin'. Load address: 0x80800000 Loading: ##error frame: 0x9ef21340 0x00000810 #error frame: 0x9ef21380 0x00000810 T error frame: 0x9ef21380 0x00000810 #error frame: 0x9ef21440 0x00000810 error frame: 0x9ef21440 0x00000804 error frame: 0x9ef21440 0x00000810 error frame: 0x9ef21440 0x00000810 ##error frame: 0x9ef212c0 0x00000810 error frame: 0x9ef21300 0x00000810 ###error frame: 0x9ef213c0 0x00000810 T T ##error frame: 0x9ef212c0 0x00000810 #error frame: 0x9ef21300 0x00000810 T #T error frame: 0x9ef21380 0x00000804 #error frame: 0x9ef21400 0x00000810 error frame: 0x9ef21400 0x00000810 T #error frame: 0x9ef21480 0x00000810 #error frame: 0x9ef212c0 0x00000810 T T #error frame: 0x9ef21300 0x00000810 error frame: 0x9ef21340 0x00000810 #error frame: 0x9ef21380 0x00000810 ##error frame: 0x9ef21400 0x00000810 #error frame: 0x9ef21480 0x00000810 #error frame: 0x9ef212c0 0x00000810 error frame: 0x9ef21300 0x00000810 #error frame: 0x9ef21340 0x00000810 #error frame: 0x9ef21380 0x00000810 ���� 2018/1/9 16:30:13 TFTP from server 192.168.10.10 ; our IP address is 192.168.10.100 Filename 'u-boot.bin'. Load address: 0x80800000 Loading: ##error frame: 0x9ef21340 0x00000810 #error frame: 0x9ef21380 0x00000810 T error frame: 0x9ef21380 0x00000810 #error frame: 0x9ef21440 0x00000810 error frame: 0x9ef21440 0x00000804 error frame: 0x9ef21440 0x00000810 error frame: 0x9ef21440 0x00000810 ##error frame: 0x9ef212c0 0x00000810 error frame: 0x9ef21300 0x00000810 ###error frame: 0x9ef213c0 0x00000810 T T ##error frame: 0x9ef212c0 0x00000810 #error frame: 0x9ef21300 0x00000810 T #T error frame: 0x9ef21380 0x00000804 #error frame: 0x9ef21400 0x00000810 error frame: 0x9ef21400 0x00000810 T #error frame: 0x9ef21480 0x00000810 #error frame: 0x9ef212c0 0x00000810 T T #error frame: 0x9ef21300 0x00000810 error frame: 0x9ef21340 0x00000810 #error frame: 0x9ef21380 0x00000810 ##error frame: 0x9ef21400 0x00000810 #error frame: 0x9ef21480 0x00000810 #error frame: 0x9ef212c0 0x00000810 error frame: 0x9ef21300 0x00000810 #error frame: 0x9ef21340 0x00000810 #error frame: 0x9ef21380 0x00000810 # 2.9 KiB/s done Bytes transferred = 356280 (56fb8 hex)