Part Number: DP83822H
Tool/software: Linux
Hi,
We are using DP83822 Phy in our MPC8360 based customized board in MII mode. We are able to see the link active (100Mbps )when connected to PC, but ping is not happening. We have verified all phy configuration registers and all seems fine. We have monitored all TX lines(TX CLK,TX_EN,TX_D0,TX_D1,TX_D2,TX_D3) and RX CLK looks fine. But no data is seen on RX lines(RX_D0,RX_D1,RX_D2,RX_D3,RX_DV). I have attached the schematic(processor side and PHY side). Please help us in resolving this issue. Following are the register values of DP83822
REG DUMP:
BMCR (0x0): 3100
PHYRCR (0x1f): 0
Strap Latch-In Register #1 (SOR1) (0x467): ffff
Strap Latch-In Register #2 (SOR2) (0x468): ffff
6266.SCHEMATIC1 _ 06_MPC8360_PCI_I2C.pdf6787.SCHEMATIC1 _ 11_DP83822_C&C_FE_.pdf