Part Number: TUSB212
Hi all,
i'm using TUSB212 in a design, and i'm trying to perform the Eye Diagram test with the oscilloscope.
The problem is that i see no differences between the test performed with TUSB212 in reset, and TUSB212 out of reset. When i de-assert the reset, the DC_BOOST/ENA_HS pin is at 0.5V, so i think it's not anymore in High Speed mode (and it isn't boosting line voltage).
It's look like TUSB212 exit the High speed mode when the USB port is in test mode.
I'm Using a Tektronix DPO 7254C with it's own USB Test Compliance Package, the Boad processor is the IMX6 Quad. The USB port is put in test mode with the Allion HSEHET B017 test fixture.
any suggestion?
thanks to all
Alessio