Part Number: TPS65981
Other Parts Discussed in Thread: LM3489, , CSD87501L, TPS6598X-CONFIG
Hello TI Team,
coming back to the discussion we had some time ago about our problem, unstable behavior with the TPS65981EVM. After a while being blocked with other tasks I picked up our Type-C PD project again and I've noticed that the current limit of the LM3489 is set to less than 1A inductor peak. Taking the ripple current into consideration the load current limit will be quite low (approx 500-600mA) causing the unstable behavior when sourcing higher demands. I've changed Radj to 24K (approx 2.8A load current) and now I can charge a Powerbook for example. Anyway, when sourcing 20V loads we use the external FET path now.
Btw, the EVM user's guide is telling that the board can power up to 60W (20V/3A). Why isn't possible to provide up to 100W by using the external path FET?
Thanks and Regards
Mario