Part Number: TPS2051B
Other Parts Discussed in Thread: TPS2041B
Hi
I am using this part TPS2051BDBV in one of my design (I have connected this switch through a 1.8V logic pin from processor ) but the Minimum Input voltage threshold mentioned in datasheet for this pin is 2.V
Will this create any potential issue during long run .Currently this logic is working fine but due to temperature variation will this create any issue ?.
What is the exact threshold above which output voltage will be switched . Board has fabricated so difficult to change logic now so please advice (let me know if a low Enable threshold part is available for this load switch which is foot print compatible )