Part Number: DS90UB914A-Q1
Other Parts Discussed in Thread: DS90UB913A-Q1
THIS IS RELATED TO THE ISSUE OCCURRING AT ONE OF MAJOR OEM NOW.
[ DS90UB914A-Q1 ] Unable to Capture CMLOUT Waveform during BIST
Hi,
My customer has found several units that are not able to capture the CMLOUT waveform during BIST mode.
- Several Units: Shown distorted camera movie. Even with BIST mode, LOSS and PASS pins are unstable. Unable to capture valid eye on CMLOUT.
- Known Good Unit: Normal camera movie. Stable LOSS and PASS pins during BIST mode and clear eye on CMLOUT. (used with same camera and cables)
From customer debug experiment, so far it's assumed that DS90UB914A-Q1 is one of the potential cause of showing the behavior above.
However, we are still looking all of the potential cause.
Do you have any ideas that DS90UB913A-Q1 could cause this kind of failure at receiver side?
I would say,
- the jitter on input PCLK to UB913A
- not enough PoC filtering on camera side would cause line/frame noise go back to the receiver side.
and so on...
Even your comments and ideas are helpful at this moment.
I know that I need to share more details which are asked on separate thread.
Thanks,
Ken