Part Number: TLK10034
Other Parts Discussed in Thread: DS100MB203
Hello,
The below figure shows the data flow path in our design:
PROCESSOR <----------> TLK10034<------------->DS100MB203<------------>SWITCH
XAUI 10GBaseKR 10GBaseKR
The configuration we want is as follows:
- TLK10034 in XAUI-to 10GBaseKR mode
- DS100MB203 as 10GBaseKR MUX( configured through SMBus)
But on board power up, the data link is not working.
We are able to access the registers of the devices TLK10034 and DS100MB203 through MXSMI and I2C respectively.
We have verified the following:
- The devices are out of reset.
- The clock of TLK10034 is proper.
- The pins ensmb(pin no:48) and MODE (pin no:21) of DS100MB203 are high.
DS100MB203 Vin voltage is 3.3V.
We have the following queries:
- Is there any fault in the configuration?
- Do we have to configure any particular registers of TLK10034?(We have a pull down resistor at ST pin to put the device in 10GBase KR)