Part Number: DS90UB947-Q1
I am using DS90UB947/948 with 2 interupt PIN
One remote interrupt pin is using INTB_IN in 948 and REM_INTB in 947. In this case, need I set C6[5] and C6[0] ? or need I read register(ISR 0xC7) to clear the interrupt?
the other interrupt will use GPIO0~3 or D_GPIO0~3? Are there any differece in GPIO0~3 and D_GPIO0~3 when used as a interrupt pin?