Part Number: DS280DF810
Team,
I am using 12 retimers (6 in transmit path and 6 in receive path).
The retimers in receive path have the eye a bit closed. So I made the following settings in RX EQ/DFE:
1. enabled VGA slection bit and
2. continuous DFE adaption.
I got an improved eye.
Now the question is what happens if I use the same setting in transmit path even though I had a good eye without these settings. I want to know the impact, if the impact is on power I don't mind.
Please let me know if there is any other impact other than that.
Thanks,
Pavan G.