Part Number: TUSB9261
Hello,
This applies to both the TUSB9261 and TUSB9261-Q1.
1) I am planing on wiring the TUSB9261 directly to a USB hub (TUSB802X) on my PCB. Can I use the Flash burner programmer to program the TUSB9261 through the hub?
2) I don't want the user to have the ability to reprogram the SPI flash. Most Flash ICs have a Write protect feature. Are there any issues with programming the Flash here at the factory with the TI flash burner software, then disabling writing on the Flash IC? If someone tries to reprogram the write protected flash with the flash burner software, will this corrupt the TUSB9261? Or would the reprogramming just be discarded?
Thanks
Tim Anderson