This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10034-DS100MB203-DS100MB203-TLK10034 LINK not up

Part Number: DS100MB203
Other Parts Discussed in Thread: TLK10034,

Hello,

The attached image shows the data path in the system.

1.When we connect the cards with TLK10034-DS100MB203 -DS100MB203 -TLK10034  back to back , the link is not up.

The register 30.15 reads 0x1803.

When we connect one card with a different card the link is up.

Why is it so? Do we have to do some specific register configuration in TLK10034?

2.When we put the switch connected to DS100MB203 in loop-back mode( Switch RX-Switch TX), then also the link is not up

Is there any particular register setting in the TLK10034 device required?

Thanks,

Ashitha