Part Number: TPS65983B
I have a Problem by creating the Thunderbolt 3 NVM.
I use:
- Application-Customization 3.17
- FM 6.43
- Imaginarium2_AR-NVM-Customization-Tool_4.4.3
- FM rev33
Hardware:
- TPS 65983b
- Alpine Ridge SP (JHL6340)
- Winbond W25Q80D
If I create the image with the low region file and the Imaginarium2 tool the result works.
If I use the Full Flash image (Region 1 offset: 0x2000 Region 2 offset: 0x20000 or 15000) the result doesn’t work, this means the Thunderbolt devices were not found.
TPS65983b_test.pjtCan you help me with that problem?
Thank you,
Patrick