Part Number: LX21EVK01
I am using the DS92LX2121/DS92LX2122 evaluation kit LX21EVK01 configured as directed in the evaluation kit for the built in self test. I would like to use the DS92LX2122 BIST register (0x24) to enable and disable the BIST. I can successfully enable the BIST by setting BIST register (0x24) bit 0 to 1, but once the BIST has been enabled no further I2C communication seems possible. as the device does not acknowledge further communication. Thus, I can enable the BIST over I2C but cannot disable it or complete any other communication once the BIST has been enabled. I run into this same I2C communication problem if the BIST is enabled using the BIST_EN pin, although communication can be resumed after the BIST has been disabled by the BIST_EN pin in this case. Is this a known problem and is there a way to stop the BIST using I2C?
Thanks