Part Number: TPS65986
Other Parts Discussed in Thread: TPS65981
Hi Sir,
I have brought Aardvark tool to configure my PD controller " TPS65986 on evaluation board of TUSB664 to disable " Multifunction Preferred " function bit using TPS6598x Utilities GUI. But here unable change registers / even its not detecting the board i feel .
Procedure i used :
1. Connected Aardvark tool SPI/I2C cable to TUSB546EVM J7 Connector
2. TUSB546EVM connected to USB Type C Cable for power ( power LEDs are glowing in TUSB546EVM device )
3. Aardvark USB cable is connected to PC and installed the USB driver .
4. Installed application TPS6598x Utilities GUI
5. Open TPS6598x Utilities GUI and checking but its not detecting .
Please help here any other settings im missing here ?
Tried I2C scanner button and its not working its showing " Beginning scan " always
My device is " TUSB564RNQEVM" SL No : 1243591 ( PD Controller TPS65986)
refereed user guide : www.ti.com/.../slva701c.pdf