Part Number: DS90UR910-Q1
We are using Des DS90UR910-Q1 with Ser DS99R421Q . What all are the additional settings required to be configured other than CONFIG[0:1] registers or gpio control .
In our test set up we have configuired I2C reg 0x01 to work in GEN 2 mode . Now lock pin is showing high but no data is received through FPD link even though clock is received . Is there any special setup or configuration to be done to work DES DS90UR910-Q1 to work in GEN 2 mode with Ser DS99R421Q.
Thanks and regards,
Anoop