This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: TPS65982DC DRP function

Part Number: TPS65982

Dear all,

In notebook application, the type C power is set as DRP.

Customer test with two notebook, when the two port connected together, which one will be the source or sink, what is the process?

Thanks.

  • Hi John,

    It's completely random when two DRP ports are connected together. It depends upon the availibility of the Rp/Rd at the instant when connection is made, which is again random.

    However, in case of one of the port prefers to take up a particular role (source or sink) then it will take up that role and the second port will take up the compliomentary role.

    I hope this answers your question. Please click This solves my issue if you think so.

    Thanks,

    Rahul