Part Number: SN65HVD1471
Hi,
SN65HVD1471 transceiver IC produces irrelevant output. To check hardware i just shorted Tx and Rx pins of IC and connected the differential pair by connecting 120 ohms across A,B and Y,Z, and given 3.3V to vcc pin and connected Gnd, Differential pairs are connected to PC via rs232 to rs422 convertor. But i haven't receive what i transmit for eg. if i send '1' i got 'g' as output. Could be please point out the mistake.