Other Parts Discussed in Thread: DS90CR287, SN65LVDS94, , DS90CF386, DS90CR288A
I am looking at the SN65LVDS93B, to replace the DS90CR287 devices I am currently using. However the SN65LVDS94 RX device does not go up to 85Mhz. What RX matching device is intended to be used with the SN65LVDS93B to allow full use of the 10MHZ -85MHz clock range. My goal is to replace the DS90CR287/DS90CR288 pair I am using with a device that ha Vccio that can be set to 1.8V, like the SN65LVDS93B.