Part Number: DP83849ID
Hello,
i have the same question as in this thread:
https://e2e.ti.com/support/interface/f/138/t/537702
-> how to Interface LVPECL correctly
unfortunately there is no answer mentiond but the topic is already closed.
I wonder about the resistor values of the thevenin Network, especially of the RX path.
At transceiver side i use 150R connected to ground as mentioned in the appnote of the AFBR-5803.
Then an AC coupling. Finally i have the option to mount a thevening Network / high impedance voltage devider or even a parallel termination.
According to the datasheet of the DP83849ID, it should be 130R to VCC (3,3V btw) and 80R to ground. But this would not lead to an DC bias of 2V LVPECL has.
It would lead to an offset of ~1,3V which fits the common known value of Vcc-2V.
But finally the Input levels of the receiver have to be fulfilled, the DP83849ID device in this case.
For fiber mode i cannot find according notes. Regarding the mentioned other thread I'm even more confused and it seems it's not clear at all.
It would great if someone can give me some advices.
Best regards
Benjamin