This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: Configuring DS90UB953/DS90UB954 for STP cable operation

Part Number: DS90UB953-Q1


Dear Sir,

It seem no specific register on 953 to set up CSI sync STP mode, the mode strap can be set as CSI sync COAX mode, not CSI sync STP mode.

On UB954 side, PORT_CONFIG(0x6d) , we can select COAX/STP and CSI mode by writing bit 2: 0 and bit1:0 by 00.

It seems MODE_SEL(0x03) on UB953 side is related with this case, but no STP or COAX option for setting, 

How to config ub953 to work as CSI sync mode and STP wire?

Thanks