This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24392: BC1.2 test fail in D+ go to Vdp_src time.

Part Number: BQ24392

Dear TI Experts,

In last post, we know that BQ24392 cannot support DCD without current source,  so my customer re-do the DCD with current source, however, it fail again. Attached is the test report, could you kindly advise

how to change test variables to pass DCD test? Thanks a lot.

BA24392 DCD with current source.pdf

  • someone is working on this issue
  • Hi Bruce,

    BQ24392 can detect more than just BCv1.2 compliant chargers but achieving this extra functionality requires a proprietary algorithm other than what is defined in the BCv1.2 specification
    •The BQ24392 proprietary detection algorithm fails the BC1.2 compliance test at the following steps:
    –7.3 step 6 requires a 14.25 kΩ - 24.8 kΩ pull down resistor from DM to GND
    •The voltage divider created by the BQ24392’s internal resistance from DM to GND and the BCv1.2 tester creates a voltage outside what the BC1.2 tester is expecting
    –7.5 step 16 requires a voltage source 0.5 V to 0.7 V on DP after a DCP has been detected by a PD
    •BQ24392 algorithm doesn’t apply this minimum 0.5 V voltage source for the duration of a DCP attachment
    –7.6 step 19 requires a voltage source 0.5 V to 0.7 V on DM and a current sink on DP
    •BQ24392 doesn’t implement this architecture
    –7.15 requires the PD to apply a 0.6 V Source on DP to indicate the SDP is detected as a dead battery
    •BQ24392 algorithm doesn’t apply the 0.6 V source on DP if a SDP is detected with a dead battery

    Regards,
    JMMN
  • Dear JMMN,
    Got it , thanks a lot for your help.