Part Number: TPS65981EVM
Other Parts Discussed in Thread: HD3SS460
Hello,
I'm trying to establish a USB3 link with two TPS65981EVM boards as described in the User's Guide SLVUAW8–August 2016 on page 10.
When doing it as shown in the picture below, then it only establishes a USB2 link, but not a USB3 link to a flash drive. I did make sure the Flash Drive is USB3 capable by connecting it directly to the PC.
I set the switches S1 as described and initially used the firmware as was at delivery of the EVM boards.
Since this did only establish a USB2 link I was looking in the TI E2E community and fond this post: 
So I tried to download the firmware mentioned there: TPS6581_HD3SS460_DRP_Source_Advanced_3_08.tpl and TPS6581_HD3SS460_UFP_Advanced_3_08.tpl but I could not find these. The Application Customization Tool seems to generate a newer version of it (4_03 instead of 3_08). When trying this, no USB link could be established to the Flash Drive. After that I tried the standard version of DFP and UFP, with this it did again only establish a USB2 link.
Which firmware should I use to establish a USB3 link?
Thank you.