Part Number: DP83867E
Hello, I am using the DP83867E Transceiver with an SGMII input. I need some help setting up the Strapping Pins. Here is what I have so far:
RX_DO Mode 4
RX_D2 Mode 4
RX_CTRL Mode 4
GPIO_0 Mode 4
GPIO_1 Mode 4
Led_2 Mode 4
Led_1 Mode 4
Led_0 Mode 4
RX_D1 and RX_D3 have same strapping pin resistors as RX_D0 and RX_D2 respectively.
Mode IDEAL Rhi IDEAL Rlo
1 open open
2 10K 2.49K
3 5.76K 2.49K
4 2.49K OPEN ( page 36 says for RX_D0, RX_D1, RX_D2, RX_D3 use Rhi 4K and Rlo 10K for SGMII)
So, I should have the following
Rhi for RX_D0,RX_D1,RX_D2,RX_D3 use a 4Kohm
Rlo for RX_D0,RX_D1,RX_D2,RX_D3 use a 10Kohm
Rhi for RX_CTRL, GPIO_0, GPIO_1, LED_2, LED_1, LED_0 use a 2.49Kohm
Rlo for RX_CTRL, GPIO_0, GPIO_1, LED_2, LED_1, LED_0 use OPEN
Please me know if I have the right resistor values.
Thanks,
Joe