Part Number: DS90UB933-Q1
Other Parts Discussed in Thread: DS90UB934-Q1EVM
Hi Teams
When we used DS90UB933 to design a camera module, we used SONY's IMX019 for the sensor.we use TI DS90UB934-Q1EVM to test the camera module. The registers of 933 and 934 are the initial configuration, without any changes. Currently, we have encountered the following problems.
1) when the sensor IMX019 is output 74MHZ @ 10bit, 933 and 934 can normally transmit and display images.And the output clock frequency of 934 doubled to 148Mhz. Is that right?
2) when the image sensor outputs 99Mhz @10bit, 933 and 934 cannot be transmitted normally, and the output image of 934 is discontinuous and incomplete, How we solve the issue? Sony's technical support team indicated that other customers used 933/934 to transmit 99Mhz normally.Do we need to configure some registers here?Which registers are critical?Our product design need 99Mhz frequency.
3) we have used 913/914,933/934 to design many products, but none of their register is configured, we are still developing 953/954. Is there any detailed configuration instructions for the register configuration, such as the sequence, configuration method in different modes and so on? This will help us a lot in developing our products. Maxin provided detailed instructions on this aspect in the earlier stage for the similar product.