Part Number: DS90UB954-Q1
Is there special register to determine what serializer is used in camera module? I would like to differentiate between 953 913 and 933 chips.
Also can 913 work with 954? What special programming needed?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB954-Q1
Is there special register to determine what serializer is used in camera module? I would like to differentiate between 953 913 and 933 chips.
Also can 913 work with 954? What special programming needed?
1. program 0x6D = 0x7F on 954
2. so I have 913 to 954, I program 0x7C = 0x80 & 0x70 = 0x1E (CSI_YUV422_8_8) on 954.
Is that correct?