Part Number: TPS65981EVM
Other Parts Discussed in Thread: TPS65981
Hello,
I wonder if it is possible to configure the TPS65981 in a way that depending on the connection with the same firmware it is possible to capture 4-lanes DisplayPort or USB3.
That means if a USB3 signal is connected it would set the switch to establish a USB3 link.
But if a DisplayPort signal is connected, all four high-speed lines would be used for DisplayPort.
Is this possible? How needs the TPS65981 be configured for that?
Thank you.
Regards,
Viktor