Part Number: DP83822IF
Other Parts Discussed in Thread: AM3356, TLK110, SYSBIOS
Hi,
We used two DP83822 to connect to PRU_MII0 and PRU_MII1 of AM3356 for PROFINET.Our problem now is one can work and one can't.
One PHY's address is 9 and the other one is 1.(Address is 9 ,RX_D2 is pullup).
The two PHY reset signals are connected together.The interesting part is that the PHY 9 always works fine(the link light is on),but PHY 1 always unable to work(the link light is off) after hardware reset .
Register 0x0001 of PHY 9 is 0x786D,Register 0x0001 of PHY 1 is 0x7849.Obviously, Auto Negotiation always failed for PHY 9.
I switched the addresses of two phys, the PHY 1 (Address is 1) always unable to work.
I think RX_D2 pullup is the key point.
It has something to do with Hardware Bootstrap Configurations.I never understood this part.
The ICEv2 board used the TLK110.Now it's replaced by DP83822.Is there anything I need to pay attention to?
Please give me some guidance.
Regards,
Andy Zhou