Part Number: DS90UB902Q-Q1
Tool/software: Code Composer Studio
Hi
I design a circuit for data transmission by DS901 and DS902 between the ECU and camera.
I used the GPIO[0:1] as UART for the communication.
as follow
And configure the 902 and 901 by I2C.
The the GPIO1 in 901 is low; The GPIO0 in 902 is low
Is that OK,Then the communication between the ECU and camera is not right
I Think the UART bus should be high in idle mode.