Part Number: HD3SS3220
Question regarding the Datasheet of HD3SS3220 (TI# SLLSES1C revised May 2017) as follows:
Referring to the datasheet HD3SS3220 (TI# SLLSES1C revised May 2017), page 22, Table 10, MODE_SELECT: The MODE_SELECT value = 00 is listed as DRP (default) which appears to contradict the note above that states: “If the default is maintained, HD3SS3220 shall operate according to the PORT pin levels and modes.” So since the HD3SS3220 has a "PORT" pin to define the default mode (UFP, DFP or DRP) should the description of MODE_SELECT value 00 be "00 - Maintain mode according to PORT pin selection (default)" instead of "00 - DRP mode (start from unattached.SNK) (default)"?